cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

EvEv_2610591
New Contributor

I tried to start GPIF mashine as in SRAM example using CyFx3BootGpifSMStart function. In debug mode CyU3PGpifLoad function return status value = 0 but CyFx3BootGpifSMStart function return value = 68. How can I fix this error? Where is error code discriptions?

0 Likes
1 Solution
abhinavg_21
Moderator
Moderator

Hi,

The above error states that: 

CY_U3P_ERROR_NOT_CONFIGURED,        /**< Object/module referred to has not been configured. */

(This error is defined in "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\fx3_sdk_1_3_3_src\sdk\firmware\include\cyu3error.h".You can refer to the source code of this API in "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\fx3_sdk_1_3_3_src\FX3\firmware\boot_fw\libsrc\cyfx3pib.c)

It seems that GPIF is not configured. Could you please share your firmware along with GPIF state machine design so that we can try to debug it here.

Thanks & Regards

Abhinav

View solution in original post

0 Likes
1 Reply
abhinavg_21
Moderator
Moderator

Hi,

The above error states that: 

CY_U3P_ERROR_NOT_CONFIGURED,        /**< Object/module referred to has not been configured. */

(This error is defined in "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\fx3_sdk_1_3_3_src\sdk\firmware\include\cyu3error.h".You can refer to the source code of this API in "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\fx3_sdk_1_3_3_src\FX3\firmware\boot_fw\libsrc\cyfx3pib.c)

It seems that GPIF is not configured. Could you please share your firmware along with GPIF state machine design so that we can try to debug it here.

Thanks & Regards

Abhinav

0 Likes