cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

gean_3054931
Contributor II

Hello,

Is fx3 supports wifi application through spi interface?

thank you.

0 Likes
1 Solution
Keerthy
Moderator
Moderator

Hello Geetha,

Please contact 'Redpine Signals' to get the driver for RS-WC-201.

View solution in original post

0 Likes
9 Replies
abhinavg_21
Moderator
Moderator

Hi Geetha anjali,

Yes you can interface Wi-Fi module with FX3 via SPI interface. But FX3 will only transmit data coming from host (PC) side to SPI side or vice-versa. It will not act as a host to the Wi-Fi module.

Thanks & Regards

Abhinav

gean_3054931
Contributor II

Hello abhinav,

it will not act as a host to the Wi-Fi module.

->what whould be the reason?

regadrs,

geethanjali.

0 Likes
gean_3054931
Contributor II

Hello abhinav

if fx3 cant act as host for wifi module, then please let me know the advantage and disadvantage of fx3 regarding this.

thank you,

geethanjali.

0 Likes
abhinavg_21
Moderator
Moderator

Hi Geethanjali,

FX3 will not act as a host because we don't have any Wi-Fi driver implementation on it.

Could you please explain in detail how are you interfacing Wi-Fi module with FX3. What are your expectations from FX3 to interact with Wi-Fi module?

Thanks & Regards

Abhinav

gean_3054931
Contributor II

Hello abhinav,

I am interfacing fx3 with RS-WC-201 Module.

how can i use this?any other option is there?

regards,

geetha.

0 Likes
gean_3054931
Contributor II

Hello abhinav.

we are interfacing fx3 with RS-WC-201 Module in spi interface.

can we use like this interface?we need to provide spi clock from fx3 to wifi module.

what do you mean by fx3 doesnot have wifi driver implementaion ?cannot we interface fx3 with wif?

if its possible to interface fx3 with wifi,which method should i use?

let me know.

regards,

geetha.

0 Likes
abhinavg_21
Moderator
Moderator

Hi Geethanjali,

Usually the driver stack is implemented on the host side. But if your Wi-Fi module has a driver stack then you can easily interface the Wi-Fi module by sending SPI commands through FX3, otherwise if you need driver implementation on FX3 then you have to approach Cypress via marketing.

Thanks & Regards
Abhinav

gean_3054931
Contributor II

Hello abhinav

driver is available from the cypress?

regards,

geetha.

0 Likes
Keerthy
Moderator
Moderator

Hello Geetha,

Please contact 'Redpine Signals' to get the driver for RS-WC-201.

View solution in original post

0 Likes