I have been using Cypress EZ USB Suite with CYUSB3014 and a J-link debugger for years without any major problems.
But recently I upgraded the tool to FX3 SDK v1.3.4, after this I can't break the execution or set any breakpoints after the execution has started.
If I press the suspend button, the button gets disabled but nothing else. I have to press stop in the console window to be able to restart the execution.
I'm not sure if this problem appeared immediately after the upgrade, but I think so.
Are there anyone that recognize this and have a solution?
BR / Joakim
Solved! Go to Solution.
Hi,
Yes there is a issue with the suspend button in FX3SDK 1.3.4. You can use old Eclipse SDK 1.3.3 with the new libraries (1.3.4) for proper JTAG debugging.
Thanks & Regards
Abhinav Garg
Hi,
I tried JTAG debugging with the SDK 1.3.4 and it is working fine for me. You can try with "Bulksourcesink" firmware example and check if there is any issue.
Thanks & Regards
Abhinav
Hi,
Yes there is a issue with the suspend button in FX3SDK 1.3.4. You can use old Eclipse SDK 1.3.3 with the new libraries (1.3.4) for proper JTAG debugging.
Thanks & Regards
Abhinav Garg