USB superspeed peripherals

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
newton_inc
USB superspeed peripherals
Hi team,  I'm  using fx3 to stream video rgb24, at 60fps i did the changes in the descriptor files,  the gpif files and the uvc files of appl note an7... Show More
fcancli
USB superspeed peripherals
Hi, I am using the CYUSB3KIT-003 EZ-USB™ FX3 SuperSpeed Explorer Kit connected to an FPGA through the GPIF interface. The transmission from FPGA to th... Show More
frankchen
USB superspeed peripherals
Hi, I am working on a project which uses FX3 to implement video application. Basically the device works fine. But when it is connected to USB 2.0 port... Show More
AKS
USB superspeed peripherals
Hi, I am interfacing a qvga sensor to my FX3 board. configured it according to AN75779 reference doc. I traced the data on wireshark and as per the ca... Show More
TeMa_2997106
USB superspeed peripherals
I want to configure the GPIF II interface of CYUSB3014 in 32-bit parallel bus + Slave FIFO mode (bidirectional). This clock frequency is stated in the... Show More
newton_inc
USB superspeed peripherals
Hi team,  I'm using cypress fx3 to stream a static test pattern as video to vlc, to check for sharpness and greyscales.  The format is         yuv 422... Show More
MiJo
USB superspeed peripherals
HI, USBBulkSOurceSink Streming example on CYUSB3KIT-003 stop blinking LED after reflash. <DEVICE>FriendlyName="Cypress FX3 USB StreamerExample Device"... Show More
AKS
USB superspeed peripherals
Hi, I have interfaced the camera sensor to FX3 board. The output data is in the YUV2 format (as default in AN75779). I want to display the data in RAW... Show More
firstLMM
USB superspeed peripherals
I complete a UVC camera with FX3 CyUSB3014 with guide of AN75779, but it works well in stream mode, but it goes bad in trigger mode; The cmos sensor w... Show More
GergelySimon
USB superspeed peripherals
Hi there, We are seeing an issue with our design that is very similar to Solved: CYUSB3014 freezes during Slave FIFO transfer - Infineon Developer Community... Show More