cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

Anonymous
Not applicable

Hi,

The 'GPIO57_I2S-MCLK_VIO3_SW' signal is connected to the I2S-MCLK pin of the CYUSB3014 device in the CYUSB3KIT-003 Superspeed Explorer kit. The signal is routed to the rectangular expansion header.

Please tell me the function of this signal.

Regards,

Prachi

0 Likes
1 Solution
ManaskantD_51
Employee

This GPIO can be used as an I2S_MCLK if you connect a I2S receiver device to the SuperSpeed Explorer Kit. If you are not using the I2S interface, you can use it as a normal GPIO too.

View solution in original post

0 Likes
1 Reply
ManaskantD_51
Employee

This GPIO can be used as an I2S_MCLK if you connect a I2S receiver device to the SuperSpeed Explorer Kit. If you are not using the I2S interface, you can use it as a normal GPIO too.

View solution in original post

0 Likes