Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals

ibka_4672506
Level 1
Level 1

Hi,

I'm starting a new product with CYUSB3014 FX3 chip.

My simple question is, how many devices I am allowed to put to the market, using Cypress default PID/VID, before having to purchase my own VID ?

My target market is not a consumer market, and 200 devices per year is the maximum number of devices I expect to manufacture in the first couple of years, So it would be very helpful if there was a way to kickstart the project with the defaut PID/VID.

Some other manufacturers (like NXP) provide custom PID to be used with their VID, and limited to a few thousands devices. Do you happen to offer a similar service?

Thank you,

0 Likes
1 Solution
YatheeshD_36
Moderator
Moderator 750 replies posted 500 replies posted 250 solutions authored
Moderator

Hello,

For Cypress FX3/FX2 devices and its variants: You cannot use the Cypress VID and PID apart from the device bootloader VID/PID for production.

USB-Serial devices are an exception.

Note:

The default VID/PID in the cyusb3 inf can be used only for testing and development purposes.

For requesting a new PID under Cypress VID, please create a tech support case: https://www.cypress.com/support

Thanks,

Yatheesh

View solution in original post

0 Likes
2 Replies
YoOb_1790021
Level 5
10 likes received 10 likes given 5 likes given
Level 5

Hi,

Is the below information for helping for you?

https://community.cypress.com/docs/DOC-10406

Best regards,

Yoichi Obana

0 Likes
YatheeshD_36
Moderator
Moderator 750 replies posted 500 replies posted 250 solutions authored
Moderator

Hello,

For Cypress FX3/FX2 devices and its variants: You cannot use the Cypress VID and PID apart from the device bootloader VID/PID for production.

USB-Serial devices are an exception.

Note:

The default VID/PID in the cyusb3 inf can be used only for testing and development purposes.

For requesting a new PID under Cypress VID, please create a tech support case: https://www.cypress.com/support

Thanks,

Yatheesh

0 Likes