- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Good day.
Now, we made our custom video camera on chip Cypress CX3 and optical sensor ov5640.
We took a "Denebola" debugging kit, its scheme and software as a sample.
During operation, the device is normally identified as a UVC device.
All the settings are available (brightness, color, resolution selection, ...)
There is communication with the sensor on the line I2C.
But there is no transmission of video information, that is, the media player window shows: 0 fps and black screen...
Please, Tell me, what could be the cause of this phenomenon?
Bad contact or lack of contact between the sensor and the cypress chip along the MIPI lane? Distortion signal MIPI?
Tell me, please, is it possible to programmatically check whether the correct mipi signal comes from the sensor OV560 to the cypress CX3?
PCB makers say they did everything right.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please go through the following troubleshooting steps and confirm.
CX3 Firmware Trouble shooting Guide
- Question
I have interfaced CX3 with an image sensor which supports MIPI CSI protocol. When I connect it to the PC and open the UVC player, I am able to see black screen. How can I fix this?
Answer:
- Probe the MIPI data & clock lanes. Ensure that they are toggling as expected.
- Is the MIPI clock gated or continuous? If the sensor is streaming in continuous clock mode, follow the steps mentioned in question 13 of the following link:
http://www.cypress.com/knowledge-base-article/cx3-hardware-frequently-asked-questions-kba91295
- Print the MIPI CSI error counts over UART by using the API “CyU3PMipicsiGetErrors”. Check if any of the error count is non-zero.
If yes, double check the sensor configuration.
- Vary the ‘thsSettleDelay’ parameter of “CyU3PMipicsiSetPhyTimeDelay()” API to check if the sensor is streaming for any of the delay
- value. Keep the first parameter as 0x01 always.
- If you were able to get zero MIPI errors and if the video is still not streaming probe the following test points
CX3 pin# | Test Signal Name |
H8 | PCLK test signal |
G6 | HSYNC test signal |
H5 | VSYNC test signal |
If only H8 toggles but not the other pins then MIPI CSI configuration may not be correct. Enter the correct values of MIPI CSI image
sensor outputs in the tool and configure the PLL dividers appropriately so that the tool will not generate any errors. Make sure to use the latest CX3 configuration tool plugins.
- Ensure that all the unused MIPI data lanes are grounded.
Probe all the three test signals (H8, G6 & H5) using oscilloscope and attach screenshot.
Thanks & Regards
Abhinav Garg
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
Hi Vladimir,
Are you facing this issue only with the custom PCB board or with Denabola kit also? Please enable the debug log messages and share the debug logs. Also probe the MIPI data lanes to check for the data.
Thanks & Regards
Abhinav
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
Good day
I added another task for MIPI errors printing:
void myThread_Entry(uint32_t input)
{
CyU3PMipicsiErrorCounts_t errorCounts;
uint32_t sum = 0;
while(1)
{
CyU3PMipicsiGetErrors (CyFalse, &errorCounts);
sum = errorCounts.crcErrCnt +
errorCounts.ctlErrCnt +
errorCounts.eidErrCnt +
errorCounts.frmErrCnt +
errorCounts.mdlErrCnt +
errorCounts.recSyncErrCnt +
errorCounts.recrErrCnt +
errorCounts.unrSyncErrCnt +
errorCounts.unrcErrCnt;
CyU3PDebugPrint (4, "\n\r mipi errors = 0x%x", sum);
CyU3PThreadSleep(1000);
}
}
I look at the output in the terminal:
mipi errors = 0x0
That is, there are no mipi errors?
If the mipi signal does not come or is distorted, will this be shown in these errors?
Many thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I modified the project code a lot:
// GpifCB callback function is invoked when FV triggers GPIF interrupt */
void esUVCGpifCB (CyU3PGpifEventType event, uint8_t currentState)
{
CyU3PReturnStatus_t status = CY_U3P_SUCCESS;
// Handle interrupt from the State Machine */
if (event == CYU3P_GPIF_EVT_SM_INTERRUPT)
{
// Wrapup Socket 0*/
if(currentState == CX3_PARTIAL_BUFFER_IN_SCK0)
{
status = CyU3PDmaMultiChannelSetWrapUp(&glChHandleUVCStream, 0);
if (status != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "\n\rGpifCB:WrapUp SCK0 Err = 0x%x", status);
}
}
// Wrapup Socket 1 */
else if(currentState == CX3_PARTIAL_BUFFER_IN_SCK1)
{
status = CyU3PDmaMultiChannelSetWrapUp(&glChHandleUVCStream, 1);
if (status != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "\n\rGpifCB:WrapUp SCK1 Err = 0x%x", status);
}
}
CyU3PDebugPrint (4, ".");
}
}
Adding line debug print:
CyU3PDebugPrint (4, ".");
Added debug in terminal output when receiving a frame.
On the denebol board there is a symbol "." output,
mipi errors = 0x0
...................
mipi errors = 0x0
...................
mipi errors = 0x0
...................
Tell me, is this correct?
But on our custom board it is not symbol ".".
mipi errors = 0x0
mipi errors = 0x0
mipi errors = 0x0
Tell me, can this indicate that we are not receiving video information on line MiPi?
Many thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Or, no......
many, many MIPI errors.....
o....
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes!
Please, see:
typedef struct CyU3PMipicsiErrorCounts_t
{
uint8_t frmErrCnt; /**< Framing Error Count*/
uint8_t crcErrCnt; /**< CRC Error Count*/
uint8_t mdlErrCnt; /**< Multi-Data Lane Sync Byte Error Count*/
uint8_t ctlErrCnt; /**< Control Error (Incorrect Line State Sequence) Count*/
uint8_t eidErrCnt; /**< Unsupported Packet ID Error Count */
uint8_t recrErrCnt; /**< Recoverable Packet Header Error Count*/
uint8_t unrcErrCnt; /**< Unrecoverable Packet Header Error Count*/
uint8_t recSyncErrCnt; /**< Recoverable Sync Byte Error Count*/
uint8_t unrSyncErrCnt; /**< Unrecoverable Sync Byte Error Count*/
} CyU3PMipicsiErrorCounts_t;
And value ctlErrCnt is very big...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Can you please print all the mipi errors individually instead sum?
As per previous response, you are seeing ctlErrCnt errors. Please confirm.
If yes, please check whether you have connected the MIPI lines properly.
0 lane of sensor with 0 lane of CX3 MIPI, 1 lane of sensor with 1 lane of CX3 MIPI, 2 lane of sensor with 2 lane of CX3 MIPI and 3 lane of sensor with 3 lane of CX3 MIPI.
Also Probe HSYNC_Test and VSYNC_Test Pins and share the active and blanking time.
If there are any mipi errors, you will not see proper VSYNC and HSYNC signals.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes.
Error ctlErrCnt occurs sometimes, but not very often.
More often it appears when connecting via USB3.
Thank you very much.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Many thanks
Now I look vsync and hsync
I wiil answer about vsyns, hsync in next post
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear,
now I look oscillograms
For example, USB3 connection, resolution 640*480, 60 fps.
Only hsync sygnal ( ? )
Freq above 30 kHz.
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
It's hsync sygnal ?
Very corrupt sinus sygnal.
No other sygnals...
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
Or It's pclk sygnal with hsync strobing....
It seems that the signal is trying to synchronize, and then the synchronization fails ...
Many thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please go through the following troubleshooting steps and confirm.
CX3 Firmware Trouble shooting Guide
- Question
I have interfaced CX3 with an image sensor which supports MIPI CSI protocol. When I connect it to the PC and open the UVC player, I am able to see black screen. How can I fix this?
Answer:
- Probe the MIPI data & clock lanes. Ensure that they are toggling as expected.
- Is the MIPI clock gated or continuous? If the sensor is streaming in continuous clock mode, follow the steps mentioned in question 13 of the following link:
http://www.cypress.com/knowledge-base-article/cx3-hardware-frequently-asked-questions-kba91295
- Print the MIPI CSI error counts over UART by using the API “CyU3PMipicsiGetErrors”. Check if any of the error count is non-zero.
If yes, double check the sensor configuration.
- Vary the ‘thsSettleDelay’ parameter of “CyU3PMipicsiSetPhyTimeDelay()” API to check if the sensor is streaming for any of the delay
- value. Keep the first parameter as 0x01 always.
- If you were able to get zero MIPI errors and if the video is still not streaming probe the following test points
CX3 pin# | Test Signal Name |
H8 | PCLK test signal |
G6 | HSYNC test signal |
H5 | VSYNC test signal |
If only H8 toggles but not the other pins then MIPI CSI configuration may not be correct. Enter the correct values of MIPI CSI image
sensor outputs in the tool and configure the PLL dividers appropriately so that the tool will not generate any errors. Make sure to use the latest CX3 configuration tool plugins.
- Ensure that all the unused MIPI data lanes are grounded.
Probe all the three test signals (H8, G6 & H5) using oscilloscope and attach screenshot.
Thanks & Regards
Abhinav Garg
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Where should I use this function?
It will be right ?
CyU3PMipicsiSetPhyTimeDelay(0x01, 0x3f);
status = CyU3PMipicsiSetIntfParams (&cfgUvcVga30NoMclk, CyFalse);
if (status != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "\n\rUSBStpCB:SetIntfParams FS Err = 0x%x", status);
}
esOV5640_VGA_config();
Thank you very much.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you very much for your answer.
Yes, the signal is only on the PCLK pin.
That is, if you follow your letter, then we have the wrong settings for the MIPI module.
But the fact is that we use a chip CX3 and a sensor OV5640. That is the same ones that are used in Denebola devkit.
Code we took the same one that is used in Denebola.
We assume that if the sensor is the same, then the MIPI settings should be the same.
Or is it wrong?
MIPI settings may vary depending on the topology of the placement of elements?
Or from release to release of products (CX3, OV5640) or any capacitors or inductors ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes settings should be same. You have to verify that the pin connections are correct.
Regards
Abhinav