How to the spi that lets me bith send and receive data simultaneously with the FX3?
You can write a function which does both transmit and receive data. You can refer to USBflashprog example provided in the FX3 sdk to see the SPI implementation for read and write
Thank you for your anster,but i mean that when i transter data the fx3 can receive data from slave at the same time.And another way is that i want to know how to set the pin of mosi to high in the idle state,because when i receive data from slave and the the slave always get the 0x00,and the slave will to responce it.