cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

ThM_3776866
New Contributor II

Hi All,

I am working cypress FX3. I changed clock setting in GPIF designer to internal clock but I am getting 190MHz of frequency. How to set Clock internal Frequency range?.

0 Likes
1 Solution
SrinathS_16
Moderator
Moderator

Hello,

The default clock values for the PIB block would be set to SYS_CLK/2, which would be 192MHz in case the SYS_CLK is 384MHz. To override this, modify the divider value in the CyU3PPibClock_t structure. Please use the following structure as parameter to the CyU3PPibInit() API.

    pibClock.clkDiv = 4;          // Clock divider is set to 4.

                                  //Modify this value to generate different clock frequencies

    pibClock.clkSrc = CY_U3P_SYS_CLK; // Clock frequency is derived from the SYS_CLK

    pibClock.isHalfDiv = CyFalse;

    /* Disable DLL for sync GPIF */

    pibClock.isDllEnable = CyFalse;

The above structure will generate a clock frequency of 100.8MHz (maximum supported on the GPIF II interface) if the SYS_CLK frequency is chosen to 403.2MHz.

Best regards,

Srinath S

View solution in original post

0 Likes
2 Replies
SrinathS_16
Moderator
Moderator

Hello,

The default clock values for the PIB block would be set to SYS_CLK/2, which would be 192MHz in case the SYS_CLK is 384MHz. To override this, modify the divider value in the CyU3PPibClock_t structure. Please use the following structure as parameter to the CyU3PPibInit() API.

    pibClock.clkDiv = 4;          // Clock divider is set to 4.

                                  //Modify this value to generate different clock frequencies

    pibClock.clkSrc = CY_U3P_SYS_CLK; // Clock frequency is derived from the SYS_CLK

    pibClock.isHalfDiv = CyFalse;

    /* Disable DLL for sync GPIF */

    pibClock.isDllEnable = CyFalse;

The above structure will generate a clock frequency of 100.8MHz (maximum supported on the GPIF II interface) if the SYS_CLK frequency is chosen to 403.2MHz.

Best regards,

Srinath S

View solution in original post

0 Likes
ThM_3776866
New Contributor II

Thank you Sir.

0 Likes