- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Immediately at startup, I get the following crash:
----
[Window Title]
GPIF™II Designer
[Main Instruction]
GPIF™II Designer has encountered a user-defined breakpoint.
[Content]
A problem caused the program to stop working correctly. Please close the program.
[Close the program] [Debug the program]
-----
I am running Windows 7 Enterprise 64 bit on a Dell Precision M4700. It is a quad i7 with integrated HD4000 graphics. If I click debug and use VS2010, I can see the following stack trace:
> KernelBase.dll!DebugBreak() + 0x2 bytes
d3d9d.dll!BreakIfNeeded() + 0x1c bytes
d3d9d.dll!CSwapChain::GetBackBuffer() + 0x1e9 bytes
wpfgfx_v0300.dll!CD3DSwapChain::Init() + 0x9f bytes
wpfgfx_v0300.dll!CD3DSwapChain::Create() + 0x113 bytes
wpfgfx_v0300.dll!CD3DDeviceLevel1::CreateAdditionalSwapChain() + 0xd9 bytes
wpfgfx_v0300.dll!CD3DDeviceLevel1::TestRenderTargetFormat() + 0x17d bytes
wpfgfx_v0300.dll!CD3DDeviceLevel1::CheckRenderTargetFormat() + 0x76 bytes
wpfgfx_v0300.dll!CD3DDeviceManager::CreateNewDevice() + 0x3fa bytes
wpfgfx_v0300.dll!CD3DDeviceManager::GetD3DDeviceAndPresentParams() + 0x251 bytes
wpfgfx_v0300.dll!CHwDisplayRenderTarget::Create() + 0x8a bytes
wpfgfx_v0300.dll!CDesktopRenderTarget::Init() + 0x244 bytes
wpfgfx_v0300.dll!CDesktopRenderTarget::Create() + 0x12d bytes
wpfgfx_v0300.dll!CMILFactory::CreateDesktopRenderTarget() + 0x116 bytes
wpfgfx_v0300.dll!CSlaveHWndRenderTarget::EnsureRenderTargetInternal() + 0x108 bytes
wpfgfx_v0300.dll!CSlaveHWndRenderTarget::Render() + 0x24 bytes
wpfgfx_v0300.dll!CRenderTargetManager::Render() + 0x4e bytes
wpfgfx_v0300.dll!CComposition::Render() + 0x28 bytes
wpfgfx_v0300.dll!CComposition::ProcessComposition() + 0x10b bytes
wpfgfx_v0300.dll!CComposition::Compose() + 0x52 bytes
wpfgfx_v0300.dll!CPartitionThread::RenderPartition() + 0x28 bytes
wpfgfx_v0300.dll!CPartitionThread::Run() + 0x60 bytes
wpfgfx_v0300.dll!CPartitionThread::ThreadMain() + 0x1c bytes
kernel32.dll!BaseThreadInitThunk() + 0xd bytes
ntdll.dll!RtlUserThreadStart() + 0x21 bytes
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Alex,
It might be the problem with installation.
Can you please try re-installing it again.
Thanks,
sai krishna.