- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Has anyone ever created an SDK project that I can use to print data read with FX3 into a txt file? - I would like to use the STREAM_IN feature of the device.
Thanks in advance
Best regards
Alessandro
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Please find the attached host application along with source code. It is a modification of the C# Streamer project which is used to obtain data from an FX3 Device.
Before starting the streamer, Make sure that the "Save to Disk" check box is ticked.
Search for the text 'mady' to see the places where the Code for writing into a text file is added.
Regards,
-Madhu Sudhan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Madhu,
Thank you so much for your support. The streamer version you sent me only works if "save to disk" check box is NOT ticked.
And actually when I tick it the streamer application stops working and sometimes it shuts down the entire OS (windows).
Alessandro Rossetta
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Alessandro,
I have made edits to the C++ streamer provided in the FX3 SDK to enable RAW data saving to files for our own device. It also works with the infinite source/sink in the "Cypress USB FX3 StreamerExample Device". You may use the code in your project if you wish: https://github.com/myriadrf/RASDR/tree/master/host/RASDRstreamer
Best Regards,
-bogdan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
i also tested the example and find the same problem when the "save to disk" is checked.
do you fix the problem in this example?
i get a exeption at
"Buffer.BlockCopy(xBufs
i add following, than i was able to write to the txt file, but only very slow
"
byte[] temp1 = new byte[Offset];
Buffer.BlockCopy(temp, 0, temp1, 0, Offset); // copy the contents received on temp[] to temp1[]
string res = string.Join("", temp1);
// Put all the data streamed to a single string
string file_name = "C:\\fx3\\test2.txt"; // Write the string to mady.txt
System.IO.StreamWriter objWriter;
objWriter = new System.IO.StreamWriter(file_name);
objWriter.WriteLine(res);
objWriter.Close();
"
after testing: the program crash every time when "Successes" has 801 reached at ""Buffer.BlockCopy(xBufs
i use win7 64bit
visual studio 2015
cu
alex
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
actually i am also facing same problem when the check box is checked C#(modified) in streamer after some time it will throw an exception so .we need to restart the operation before reaching that limit .if any one able to do this please help me also.it will very helpful to me