cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

Anonymous
Not applicable

Hi,

   

I am new to deal with USB controller. When I followed application notes AN65974 to try loopback example using synchronous slave fifo interface, I found a problem. When I using Control Center to transfer 1024 bytes from PC to FPGA by Transfer File Out, the whole loop worked well. However, if I trying to transfer a few bytes of data (such as 8 bytes) from PC to FPGA, then data cannot be transferred back. The error code is 997. 

   

I want to know where is the problem? And may I do some modifications on the loopback firmware to allow me to send few bytes to FPGA?

   

 

   

Regards

   

Zoe

0 Likes
2 Replies
Anonymous
Not applicable

Hi,

   

The loopback should work for small chunk of bytes as well. If it doesn't can you make sure that the PKTEND signal is being properly connection. (This is the signal which marks end of transfer for short transfers from FPGA to FX3).

   

Please create a tech Support case.

   

Regards,

   

-Madhu Sudhan

0 Likes
XiXI_4139851
New Contributor II

HI

I have encountered the same problem, have you solved it?

Regards   

Xie

0 Likes