cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

PrN_4452166
New Contributor II

Hi,

I am Using FX3 and the Image sensor processor OV426, The Both FX3, and the Processor are isolated by the digital isolator, 

My Doubt is Where I need to place the series resistor Near the FX3 or Processor. Because the Series resistor should be placed near to the Source. Here My Image sensor processor us a source.

Where I need to place. Near FX3 or Near to the Processor after isolator?

0 Likes
1 Solution
YashwantK_46
Moderator
Moderator

Hi,

If the image sensor and FX3 are placed at a distance apart from each other, the series resistors need to be placed near to the FX3.

But if they are very near such that you dont have space to put them near FX3, then you can put them near the image sensor processor.

Regards,

Yashwant

View solution in original post

1 Reply
YashwantK_46
Moderator
Moderator

Hi,

If the image sensor and FX3 are placed at a distance apart from each other, the series resistors need to be placed near to the FX3.

But if they are very near such that you dont have space to put them near FX3, then you can put them near the image sensor processor.

Regards,

Yashwant

View solution in original post