FX3 SDK v1.2 with old GPIF II Designer

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

It appears that the FX3 SDK v1.2 comes bundled with an old release of the GPIF II Designer (v1.0, 3/1/12).  It doesn't appear that I can install the latest GPIF II Designer without uninstalling the complete SDK.  Is there a way around this?  Can we get an updated SDK that includes the latest GPIF II Designer?

0 Likes
3 Replies
Anonymous
Not applicable

I have the same problem! Unable to update it with update manager. Unable to update it at all (Win-7 64-bit). Unable to install sdk without designer.

0 Likes
Anonymous
Not applicable

There are no changes to the GPIF II designer. That is the reason why they have kept the same old version with the latest SDK v1.2

0 Likes
Anonymous
Not applicable

The Release Notes for v1.0.1 indicate there are differences between the latest GPIF II Designer (v1.0.1) and the one supplied with the lastest SDK (v1.0).

   
        
  • Updated the Asynchronous and Synchronous FIFO 2 bit project in Cypress Supplied Interfaces....
  •     
  • Added support for overriding the interrupt pin of p-port....
  •     
  • Added “Number of States” field for displaying the number of states....
  •     
  • ....
  •    
0 Likes