Hello,
Is there a way to set the (Serial Number) SN in the device properties it is currently set to nothing.
Solved! Go to Solution.
Hello Miguel ,
yes, you can change the Serial number string from the USB descriptor on the firmware.
From an application perspective, If you need to differentiate the two devices on your application means you can use the device path on windows.
Thanks & Regards,
Shanthakumar
Can you elaborate more ?
Hello,
Yes I would like to run two FX3 chips simultaneously on the same computer on two USB 3.0 ports. So what would be the best way have an identifier, such as a serial number? Would I need to have two sets of firmware, if the firmware does need to change? I can see in the cyfxusbenumdscr.c file you can change the /* Serial number string index */ value. What would be the best approach? Thank you.
Best Regards,
Miguel Villasana
Luxima Technology LLC
Hello Miguel ,
yes, you can change the Serial number string from the USB descriptor on the firmware.
From an application perspective, If you need to differentiate the two devices on your application means you can use the device path on windows.
Thanks & Regards,
Shanthakumar