cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

QsLi_3517121
New Contributor

Can EZ-USB FX3 be simultaneously emulated as a video device and a serial device?

Is there an example of emulating two devices with EZ-USB FX3?

0 Likes
1 Solution
SrinathS_16
Moderator
Moderator

Hello,

FX3 can be used to enumerate two devices simultaneously.

The FX3 SDK provides separate examples of UVC class and CDC class. I have attached a project which uses the UVCVideoClassBulk and UsbUart examples from the SDK. This firmware enumerates the device as CDC and UVC interfaces.

Please note that the device descriptor is modified only for the SuperSpeed operation. The HS descriptors can also be modified in the same way to operate in USB2.0 mode.

Best regards,

Srinath S

View solution in original post

0 Likes
1 Reply
SrinathS_16
Moderator
Moderator

Hello,

FX3 can be used to enumerate two devices simultaneously.

The FX3 SDK provides separate examples of UVC class and CDC class. I have attached a project which uses the UVCVideoClassBulk and UsbUart examples from the SDK. This firmware enumerates the device as CDC and UVC interfaces.

Please note that the device descriptor is modified only for the SuperSpeed operation. The HS descriptors can also be modified in the same way to operate in USB2.0 mode.

Best regards,

Srinath S

0 Likes