cancel
Showing results for 
Search instead for 
Did you mean: 

USB superspeed peripherals

Will_lee
New Contributor II

我在使用CYUSB3014的过程中,将芯片配置为了USB3.0 + UART模式,然后遇到两个问题

1> 在32位总线下 UART的TX和RX配置在GPIO55 和 GPIO56 ,是否可以再 GPIO54上实现 UART_RX ?

2> 在32位总线下,UART和SPI可以同时使用吗?

0 Likes
1 Solution
YiZ_31
Moderator
Moderator

1> 在32位总线下 UART的TX和RX配置在GPIO55 和 GPIO56 ,是否可以再 GPIO54上实现 UART_RX ?

=>不可以

2> 在32位总线下,UART和SPI可以同时使用吗?

=>32位总线下没有SPI引脚

View solution in original post

1 Reply
YiZ_31
Moderator
Moderator

1> 在32位总线下 UART的TX和RX配置在GPIO55 和 GPIO56 ,是否可以再 GPIO54上实现 UART_RX ?

=>不可以

2> 在32位总线下,UART和SPI可以同时使用吗?

=>32位总线下没有SPI引脚

View solution in original post