Downloaded project from git and trying to build with command
cs-make
build job failed with below error as it is unable to find the fx3.ld from current path. when checked the makefile it was showing the workspace path which the developer used and pushed to git
so we imported the same project in eclipse and now build executed success and the makefile was updating to the current working directory.
is there a way to change the path in makefile without importing the project in eclipse.
Solved! Go to Solution.
Hello,
Please refer to the following KBA to understand the detailed steps to be followed to build FX3 project using command prompt:
The KBA also mentions the modifications that should be done on the makefile. Please refer to the KBA mentioned above and make the required modifications on the makefile to build the project using command prompt.