Hi Everyone,
Our customer is using CY7C68300C with CF card along with the 56_bus_HDD.iic configuration which can recognized as local drive under Windows.
We attempted configure the drive as removable drive using 56_bus_cf.iic/56_bus_md.iic but unable to find the storage media.
Can anyone comment how we can modify the configure/iic file based on HW similar CY4615B so that we can access the drive and media as removable drive?
Thanks and Regards,
Kevin
Solved! Go to Solution.
Hi Kevin,
-Could you please program the 56_bus_cf.iic/56_bus_md.iic file on the CY4615B and check if the drive is detected?
-Please ensure that DRVPWRVLD bit is enabled in the settings. If only a CF card is connected, please disable the SEARCH_ATA_BUS bit.
Best Regards,
Sananya
Hi Kevin,
-Could you please program the 56_bus_cf.iic/56_bus_md.iic file on the CY4615B and check if the drive is detected?
-Please ensure that DRVPWRVLD bit is enabled in the settings. If only a CF card is connected, please disable the SEARCH_ATA_BUS bit.
Best Regards,
Sananya