cancel
Showing results for 
Search instead for 
Did you mean: 

USB low-full-high speed peripherals

Anonymous
Not applicable

I have no experience with cypress and want to program a USB FX2LP CY7C68013A. I read that with EZ-USB FX2LP USB2.0 Develope Board Logic Analyzer Module bought on ebay can be programmer. I dont know if there is an adapter for CY7C68013A with 56 pins or in what way do the connections between CY7C68013A pins and the programmer. I would also like to know if are some specific pins which must be used or if they are all chip pins.

0 Likes
2 Replies
AjayB_76
Moderator
Moderator

There are 2 methods to program the FX2LP.

   

a) Download from USB - The code can be loaded onto FX2LP from the USB interface itself.  

   

b) Boot from EEPROM- Once code development is complete, the binaries can be loaded onto EEPROM and then system can boot from the EEPROM. 

   

The document below has the details:

   

http://www.cypress.com/documentation/application-notes/an50963-ez-usb-fx1-fx2lp-boot-options

   

I am not sure which is the programmer you are referring to on ebay, pass the link and i can do a quick check.

0 Likes
Anonymous
Not applicable

If I have a circuit with a fx2lp and eeprom working. I can copy the information from eeprom and write in a new eeprom, fx2lp works as the original circuit?

0 Likes