cancel
Showing results for 
Search instead for 
Did you mean: 

USB low-full-high speed peripherals

rsg_chrisc
New Contributor

We've encountered an issue with the CY7C65213 that only seems to manifest with the CypressSerial (CDC) driver as shipped in the USB Serial SDK (driver version 3.13.0.59 dated 13 Oct 2015) - under specific circumstances, the CY7C65213 stops forwarding data from the connected device to USB, but is still responsive to DTR control events from the USB host.

We're aware that there's an updated driver available (version 3.13.0.84, dated 17 Jan 2018) that fixes the issue as we've seen, but there's no updated version of the USB Serial SDK or downloads of updated drivers so we can tailor it for our custom VID/PID.

How/Where can we get the updated CypressSerial (CDC) driver for such tailoring?

0 Likes
1 Solution
1 Reply