USB hosts hubs transceivers

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
Robin_Peng
USB hosts hubs transceivers
您好,目前使用CYUSB3304-68LTXI进行设计,已经上板进行测试,在做高低温实验时,发现在-40度出现USB报错,当温度回到20度时,USB又恢复正常。请问这是由什么原因造成的,谢谢 Show More
Dimitry
USB hosts hubs transceivers
Hi  our system is NVIDIA Jetson Xavier NX  when USB3.0 SSD unplug form Jeston " native USB3 port", OS can show unplug device information. but when USB... Show More
NXTY_Nishinaga
USB hosts hubs transceivers
Hello, I have a question about the operation of DSx_PWREN ( or PWR_EN) in CYUSB33xx and CYUSB230x. When is DSx_PWREN ( or PWR_EN) turned On/Off ?  Wha... Show More
Mitchell_shen
USB hosts hubs transceivers
  We are use HX2VL USB2.0 Hub on our system. But our system has low power requirement for USB ports. Does HX2VL meet below mention of LPM & BESL suppo... Show More
TeMa_2997106
USB hosts hubs transceivers
I once asked the following question.https://community.infineon.com/t5/USB-hosts-hubs-transceivers/Signal-quality-measurement-in-HX2LP/m-p/322491 After... Show More
kalauffenburger
USB hosts hubs transceivers
Hello, I have essentially the same question that was addressed in this post: CY7C65631 linux compatiblity and few questions. It has a disposition of ... Show More
TeMa_2997106
USB hosts hubs transceivers
The Overcurrent detection in the CY7C65630 datasheet has the following description:After detecting an overcurrent condition, hub reports overcurrent c... Show More
drko001
USB hosts hubs transceivers
Hello, We are currently in development of a product implementing HX3 CYUSB3304 USB hub. We configured the hub as I2C slave to be configured from an ex... Show More
TeMa_2997106
USB hosts hubs transceivers
Is it a problem if the absolute maximum rating of input voltage -0.5V is violated even for a short time? The undershoot of the input signal of a pin i... Show More
Augustine_Yeh
USB hosts hubs transceivers

Hi Cypress

We need CYUSB3314 firmware( bin file) for disabled U1 and U2 , Can you provide it to us, Thank !!

 

Forum Information

USB hosts hubs transceivers

Discussion forum regarding USB hosts hubs and transceivers topics.
Top liked authors