- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
For my given application, I need to have more than 2 downstream USB Type A Super Speed+ Ports. Here is the list of Downstream ports as described in the datasheet:
As there are 3 USB-C connections with 10GB/s bandwidth, I was wondering if it is possible to use these with a Type-A connector? Such as the connector shown below:
My configuration would end up looking like:
DS1, DS3, DS4, DS5 -> USB A
Thank you,
Greg
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Greg,
I checked with our internal team and it should be possible to make DS2, DS3 as Type-A only. You could add external termination on one of the CC pins for each port and connect the corresponding set of the superspeed lines from the hub to your connector, the other of lines can be left floating.
Please let us know if the upstream port is going to be a Type-C port. If not, even that would need external termination on the CC pins to take care of the superspeed lines.
Best Regards,
Sananya
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Greg,
It is possible to convert the Type-C and PD ports DS1, DS2, DS3 to a Type-A port. However, since DS1 is also PD capable, you would have to modify the firmware to disable the PD features. The HX3PD firmware project can be found at- https://www.cypress.com/documentation/reference-designs/ez-pd-ccgx-usb-type-c-monitordock-solution
I would suggest using DS2, DS3 as Type-A ports instead since this can be done by modifying the port configuration using the HX3PD Configuration Utility. Please note that this is included in the "Hub Controller" part of the configuration so we would be providing the modified file to you.
We have not tested this configuration on our hardware so please let me know if its a requirement and I will verify internally if any additional steps are needed.
Best Regards,
Sananya
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for the quick reply!
Would it be best to use TX1/RX1 and not connect TX2/RX2? Or should I do something with TX2/RX2 like pull them to gnd with a resistor?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
@Sananya_14 this is a requirement for the project. If you could get that information, it would be greatly appreciated!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Greg,
I checked with our internal team and it should be possible to make DS2, DS3 as Type-A only. You could add external termination on one of the CC pins for each port and connect the corresponding set of the superspeed lines from the hub to your connector, the other of lines can be left floating.
Please let us know if the upstream port is going to be a Type-C port. If not, even that would need external termination on the CC pins to take care of the superspeed lines.
Best Regards,
Sananya
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hey Sananya,
The application will be using upstream USB-C, thank you!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Greg,
In that case, you would only need to make the above mentioned hardware changes on the Type-C DS ports (except for DS1 which would require the PD to be disabled in the firmware) to change the port to Type-A.
Best Regards,
Sananya