Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

你好!

   

我司做的一款产品使用贵司CYUSB301X进行设计,设计中遇到一些问题在坛子里咨询一下。

   

遇到的问题如下:

   

1、使CYUSB301X处于Async Slave FIFO工作模式,数据位设置为8位。

   

(1)地址位A[1:0]是不是就是FIFO的地址?

   

(2)地址位A[1:0]的引脚设置是使用GPIO[9:8]还是GPIO[29:28]?

   

(3)FIFO进行切换时是需要外部CPU进行A1/A0进行设置,还是可以进行软件寄存器设置进行切换?

   

2、时钟配置引脚FSLC[2:0]是不是可以直接连接到GND?(3个引脚不做弱下拉处理)

   

3、VBAT作为电源引脚是否可以悬空处理?还是必须连接到VBUS?

   

4、CYUSB3011和CYUSB3013的buffer size具体有多大?有几块buffer?

   

谢谢!

   

 

   

LEO

0 Likes
3 Replies
Anonymous
Not applicable

1.地址位A[1:0]是不是就是FIFO的地址?

   

1A: 是的。

   

2)地址位A[1:0]的引脚设置是使用GPIO[9:8]还是GPIO[29:28]?

   

2A) 使用GPIO[29:28], 请参考CYUSB3014 datasheet。

   

3)FIFO进行切换时是需要外部CPU进行A1/A0进行设置,还是可以进行软件寄存器设置进行切换?

   

3A)需要外部CPU 对A1/A0进行设置。

   

2、时钟配置引脚FSLC[2:0]是不是可以直接连接到GND

   

A2:如果全部设置为000, 可直接接地, 如果接电源,需要做弱上拉处理。

   

3、VBAT作为电源引脚是否可以悬空处理?还是必须连接到VBUS?

   

A3:推荐和VBUS 一起链接。

   

4.CYUSB3011和CYUSB3013的buffer size具体有多大?有几块buffer

   

A4:CYUSB3011的 SRAM:256KB, CYUSB3013 的SRAM :512KB。

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Liujun,你好!

   

问个问题,如果我将FIFO地址引脚A[1:0]连接到GND,那么CYUSB301X工作在Async Slave FIFO工作模式下时,做数据缓存的FIFO只要1个,其FIFO大小有多大?另外如下图所示的工作模式该如何进行寄存器配置?

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi,

   

在GPIF II界面上设置async slave fifo工作时,界面提示的FIFO地址引脚提示的是GPIO8和GPIO9,不是GPIO28和GPIO29?

0 Likes