cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

when the  CYUSB3014 is used  as HS-OTG host, how can I set  up the FX3 device? There is nothing about  CYUSB3014 is used  as HS-OTG host in FX3APIGuide.pdf.I want to understand  how HS-OTG host work on CYUSB3014?Thank you!

0 Likes
2 Replies
Anonymous
Not applicable

That part of the SDK isn't exposed yet. Please create a tech support case (MyAccount -> MyCases) so that we can understand your requirement better and make sure it is addressed properly.

   

Regards,

   

Anand 

0 Likes
Anonymous
Not applicable

Please note that we have released our FX3 SDK with the following link(http://www.cypress.com/?rID=57990). After installed it, you can find some development resources in the path C:\Cypress\Cypress SuperSpeed USBSuite.

You can also find some useful files in the path C:\Cypress\FX3 SDK if you have installed CYUSB3KIT-001 EZ-USB FX3 Development Kit (http://www.cypress.com/?rID=58321).

   


       These are  replies from Cypress company.But my question is not resolved ,because I have done like that long time ago!
 

0 Likes