cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

Hi

   

I want to transfer data from two ADC (ads1298 24-bit, 8-channel ADC chip with SPI interface) to my pc.can I use CYUSB3KIT-003 for SPI connection ? and because I want to sample signal , I need usb 3

0 Likes
1 Reply
Anonymous
Not applicable

Hi,

   

Yes. You can use the CYUSB3KIT-003 kit for SPI Connection. But the SPI Lines are multiplexed with UART lines on that board which goes into a USB UART converter on that board. So it is recommeded that you remove this chip before testing the SPI interface/.

   

The SPI of Fx3 can go upto 33 Mhz.

   

Regards,

   

-Madhu

0 Likes