cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

fedo_1531736
New Contributor

Two cypress devices used in my system. one is CYUSB3014 and the other is CY7C68013. Can I use the same library for the SW develop to control the two device.

0 Likes
2 Replies
Anonymous
Not applicable

Which driver are you using for CY7C68013. Our latest driver is CyUSB3.

   

You can use the same libraries for writing host application for CY7C68013 or CYUSB3014. Please quickly first try by using Cypress Control center application to confirm that the transfers are happening on both the devices.

0 Likes
fedo_1531736
New Contributor

Hi Nishant,

   

    Thanks for your quick reply. 

   

    Yes. Both devices use the same driver CyUSB3, and they both can be controlled by the Control center.

0 Likes