Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

saku_4625426
USB superspeed peripherals
Hello Community,Can we pass vendor requests without using control center i.e..,can we make it automatic in code itself?Let me know whether this is pos... Show More
WGT_4383351
USB superspeed peripherals
Set the TimeOut to 10 seconds. Then use XferData() to read 2KB data from an IN endpoint, then the wait begain since there is no data available.Then 2K... Show More
WGT_4383351
USB superspeed peripherals
In AN87216:The expected behavior when PC only send data to master FX3 but doesn't read data from slave FX3 is : When data is send from PC to master FX... Show More
saku_4625426
USB superspeed peripherals
Hello Community,I want to toggle the GPIO pin(In my case it is GPIO 57) in order to increase the voltage going to S0-Port.I am using custom FX3S board... Show More
HaHu_4486526
USB superspeed peripherals
Hi:  i want to read and write a 8bits byteaddr I2C device by USB3014, i can write  the right slave addr and sub-addr, but i find wirte data is fail.th... Show More
LuTa_4642501
USB superspeed peripherals
Jlink server doesn't find my board:JLinkGDBServer -device ARM9SEGGER J-Link GDB Server V6.62d Command Line VersionJLinkARM.dll V6.62d (DLL compiled Ma... Show More
sach_4661001
USB superspeed peripherals

您好:

FX3增加I2C EEPROM

請問哪裡可以取得CODE,燒入EEPROM可讓FX3可以WORK?

感謝

SaLe_1201446
USB superspeed peripherals
Dear all, I am using the FX3-USB3014 to capture MPEG2 TS data from LG electronics demodulator IC. Because there is no flow control mechanism between F... Show More
PhMi_4136011
USB superspeed peripherals
Hi,We are working with an 10 bit RAW gray scale sensor and established a Video stream (1080p 30fps, WIn10). SeeRe: Setup MIPI connection between CX3 and OV2740... Show More
RiFu_3006586
USB superspeed peripherals
Hi,i have a Enclustra PM3 with Mars ZX3 Zynq 7000 SoCOn PM3 Board a FX3 3014  is assembled.Because of the given schematic I can't use GPIO29 als FV Pi... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.