Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

EmJo_4807876
USB superspeed peripherals
Hi, I'm working on a project that involves modification of the mass storage functionality implemented on the CYUSBFX3KIT-003 by moving the storage mem... Show More
HuYa_4249091
USB superspeed peripherals
Hi, I've enabled the Exposure Time(Absolute) in USB Camera Terminal Descriptor & corresponding FW code, and it worked. I tried to add Auto Exposure Mo... Show More
chsh_1759911
USB superspeed peripherals
i want to use cy3014 to control my FPGA PS configure sequence i want to control spi flash output FPGA config data (MISO connect with FPGA data pin too... Show More
Raeleen
USB superspeed peripherals
Hi, I am developing an oscilloscope in-house. Currently, I am working on the Texas Instrument's ADS54J60evm and TSW14J56evm boards. My end goal is to ... Show More
yaqi_4776616
USB superspeed peripherals
hello, I created a CX3 project, I observed the sensor output with an oscilloscope, and my sensor configuration was successfully able to output the exp... Show More
yaqi_4776616
USB superspeed peripherals
Hello I currently have a CX3 project configured, I downloaded it to the CX3 hardware and started the CP camera, the camera's still image and Video ico... Show More
ReA_3297666
USB superspeed peripherals
Hello we are using CX3 RDK board receive a RAW 10bit MIPI sensor Input, We made the configuration as shown below  In the image configuration , the ne... Show More
cnlohr
USB superspeed peripherals
I have a basic setup working great with the FX3 when operating in synchronous master mode with internal clock settings.  But, my data source always ha... Show More
haxu_299926
USB superspeed peripherals
 Jump to solution Hi,         PleaseTell me whether I can modify the CX3 GPIF state machine by myself,and Is there an example that supports u3vis... Show More
TeMa_2997106
USB superspeed peripherals

What is the maximum depth of endpoints that can be configured on FX3?

Thanks,
Tetsuo

Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.