Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

FCO_ereca
USB superspeed peripherals
Hello, I need to send 2 simultaneous streams on USB, among 4 MIPI-CSI signals.Is CYUSB3065-BZXI suitable for this application? Thank you Show More
GrCa_1363456
USB superspeed peripherals
Does Infineon have an example that supports USB 3.x to JTAG? A USB SuperSpeed (3.0) to JTAG would support downloading an image to an FPGA without sett... Show More
AKS
USB superspeed peripherals
Hello all, I need to start a slave device which has SPI control lines interfacing with FX3 (CYUSB3KIT-003) with separate data lines (D0...D8) somethin... Show More
Simon_Shi
USB superspeed peripherals
Hi all, I am looking for USB FX3 SDK version 1.3.5  as mentioned in KBA218830,but i can just find version 1.3.4  from the following link: https://softwaretools.infineon.com/tools/com.ifx.tb.tool.ezusbfx3sdk... Show More
kgkang
USB superspeed peripherals
I have problem to discard DMA buffer. I'm receiving data using isochronous transfer.  I have tested data receiving GPIF to USB isochronous transfer mo... Show More
jl46
USB superspeed peripherals
FX3 SPI Flash
solved msg Solved
Hello, Is the FX3 (CYUSB3014) limited on the above mentioned SPI flash devices? Is it possible to use existing SPI flash in control center and other ... Show More
hongliangli
USB superspeed peripherals
你好:           请问我用上位机控制cyusb3014传输数据,每次初始化*USBDevice指针时,都会消耗很长时间,大概15-20ms左右呢?以下是上位机初始化的程序。 CCyUSBDevice *USBDevice = new CCyUSBDevice();CCyControlEnd... Show More
Doug
USB superspeed peripherals
Hi, I'm using the FX3 to interface with 3 10-bit image sensors and send the data via USB. Sensor data is synchronized into a 30-bit word via an FPGA c... Show More
aleb_4846776
USB superspeed peripherals
I am using the AN75779 firmware code. When I add a new extension unit and modify the connection between the different units, Windows recognizes the de... Show More
Lee_sin
USB superspeed peripherals
Hello, I encountered some problems in the process of reading and writing FPGA and FX3. I want to clarify, the configuration is as follows:The size of ... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.