Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

   

I am trying to understand if it is possible to configure an FPGA using GPIF II (32-bit slave selectMAP) which requires the GPIF be configured as Master mode. Then switch GPIF to slave FIFO mode. I am wondering if you have an example.

   

Based on my understanding, in my case I cannot have disjoint state machines because one is master and one is slave. So, if I define two separate GPIF II projects, how I should configure the chip after completing the FPGA configuration? At the moment when I load a firmware to cypress, I cannot load any other firmware until a power down then up happens.

   

Also, I need to have an enable/disable signal along with the data path to implement a non-continuous FPGA configuration. If I choose any available GPIO, will it be synchronze with the data (for instance, it will be working with PCLK = 80MHz rate)?

   

Thanks,

   

Nazila

0 Likes
1 Reply
Anonymous
Not applicable

 Hi Nazila!

   

you can and have to reload the GPIF II designs just use see post disable and load function gpif functions.

   

http://www.cypress.com/?app=forum&id=167&rID=60662

   

You also can choose a better configuration for more GPIF designs at the designer, see post... Then you do not have to rename the configuratin structures all the time.

   

http://www.cypress.com/?app=forum&id=167&rID=60039

   

 

   

For enable and disable use one of the 32 bit data lines if you just need 16-bit data for fpga configuration.

   

Hope this helps out.

   

Regards 

   

Lumpi

0 Likes