cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

Hello,

I want to read/write I2C EEPROM on the FX3 board with UsbI2cRegMode example firmware project.
But I couldn't understand the process.

Project readme file says,
" The device enumerates as a vendor specific USB device with only the control endpoint and provides a set of vendor commands to read/write the data on I2C EEPROM devices.".

   

That's all. There is no additional information how it can be realized.

When I look over "CyFxUSBSetupCB" callback function and "CyFxUsbI2cTransfer" function,
 I can produce callback function's "setupdat0" and "setupdat1" parameters.

1. How can I generate vendor commands with "setupdat0" and "setupdat1"?
2. How can I send vendor commands within "USB Control Center"?
3. When I send a read command, how can I observe the data?
4. When I want to write to EEPROM, how can I send the EEPROM data?

I would appreciate, if someone help me.

Regards,
Ali

0 Likes
2 Replies
LiMa_282146
New Contributor II

Hi

   

              

   

In the USB Control Centre highlight the control endpoint, click on the data transfer tab and then enter values in the following fields to suit your application

   

Direction                Out/IN you decide

   

Req Type               Vendor

   

Target                      Device

   

Req Code              Your Vendor code

   

wValue                    you decide

   

wIndex                     you decide

   

USB setup data is an 8 byte array sent by the host pc and these are stored in setupdat0 and setupdat1 which the firmware then parses to decode the control information contained in the setup data. In the eeprom example (cyfxusbi2cregmode.c) this is done in the following code

   

 /* Parse the control request parameters. */

   

    attr    =  (uint8_t) (setupdat0 & 0x000000FF);

   

    rqt     =  (uint8_t)((setupdat0 & 0x0000FF00) >> 8);

   

    value   = (uint16_t) (setupdat0 >> 16);

   

    index   = (uint16_t) (setupdat1 & 0x0000FFFF);

   

    length  = (uint16_t) (setupdat1 >> 16);

   

 

   

attr is the request type and will be set by Control Centre when you select Vendor.

   

rqt is the users vendor code and in this example for an eeprom read the code shows

   

 case CY_FX_RQT_I2C_EEPROM_READ:

   

            i2cAddr = 0xA0 | ((value & 0x0007) << 1);

   

            CyU3PMemSet (glEp0Buffer, 0, sizeof (glEp0Buffer));

   

            status = CyFxUsbI2cTransfer (index, i2cAddr, length,

   

                    glEp0Buffer, CyTrue);

   

            if (status == CY_U3P_SUCCESS)

   

            {

   

                status = CyU3PUsbSendEP0Data(length, glEp0Buffer);

   

            }

   

            break;

   

 

   

If you look in cyfxusbi2cregmode.h you will see that this is defined as 0xBB

   

 Likewise the value field in this example is the eeproms address while index give the internal eeprom offset address.

   

 To read the eeprom then the following data is put into Control Centre

   

Direction                 IN

   

Req Type                 Vendor

   

Target                      Device

   

Req Code               0xBB

   

wValue                    try 0x0000 but depends on how the eeprom address pins are set

   

wIndex                     0x0000

   

 In the Bytes to Transfer Box type in the number of bytes you want to read.

   

Hope this helps.

   

Sodafarl

0 Likes
Anonymous
Not applicable

Hi Sodafarl,

Your answer was very clear and it worked. Thanks for your help.

Regards,
Ali

0 Likes