Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lechc_282591
Level 4
Level 4

Hello, everyone,

   
    I have downloaded the firmware into the I2C EEPROM. It is working well. Now I want to update the firmware in the same EEPROM chip. This will be very useful for our customers. Is it possible? When I reset the DVK board, it will automatically boot from the I2C EEPROM and the message ”Please reset your device to download firmware” will pop up if  I try to download a new firmware to the I2C E2PROM in the USB Control Center. How can I achieve that? Any suggest will be appreciated.   
   
    Thank you very much.   
   
        
   
    Best regards,   
   
    Lehua Chen     
0 Likes
1 Reply
Anonymous
Not applicable

Hi,

   

You could do one thing with the DVK. You can just remove the J42 and press the reset button. Then Control Center recognizes your device as a default bootloader device. Then put the jumper back on J42 and try programming the DVK.

   

Reagrds,

   

sai krishna.

0 Likes