cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

Hi,

   

What are the steps to start a new firmware in Eclipse from scratch? Do I need to install sourcery G++ in order to build my firmware codes on the Eclipse?

   

Thanks,

   

Nazila

0 Likes
7 Replies
Anonymous
Not applicable

Please look at chapter 9 of FX3 programmers Manual.

   

Regards,

   

Anand

0 Likes
Anonymous
Not applicable

Hi,

   

I already looked at it but it only explain how to import the already written projects. My problem now with the new project is the <cyu3... .h> files are not recognized by the compiler! Even though I already added the FX3 SDK library (FX3 SDK/firmware/u3p_firmware/inc).

   

Thanks,

   

Nazila

0 Likes
Anonymous
Not applicable

I think I found what the problem was! I added the path to the Cypress library files to the project's "includes" but not to the file's "includes" which is very weird, I expect that when I add the path to the project, automatically the files inside that project see the path!

   

Anyway, now the project can compile.

0 Likes
Anonymous
Not applicable

I started a new project and only add new files from the already compiled folder of cypress: BulkLoopAuto. I encounter the same problem: cyfxbulklpauto.c does not recognize the cyfxbulklpauto.h and even after I add explicitly the path of the own project (where both of these files exist), the project compiles but there is no elf file generated.

0 Likes
Anonymous
Not applicable

Another error that I get is

   

Cannot find builtin/gnu.mk

   

Has anyone create a project (NOT importing already built projects from the firmware folder). I think I am missing some settings, ...

   

Anyone can help?

0 Likes
LiMa_282146
New Contributor II

Hi,

   

I have used an existing project, USBBulkLoopAuto as a template for a new project. I've outlined the steps below

Go to the firmware/basic_examples folder and make a new folder with your project name, for example my_proj.

   

Open the cyfxbulklpauto folder and copy all the files into the my_proj folder - do not copy the debug folder if there is one.

   

You will then need to rename three source files. Rename cyfxbulklpauto.c to my_proj.c,  cyfxbulklpauto.h to my_proj.h and cyfxbulklpdscr.c to my_projdscr.c

   

With a text editor open my_proj.c and change the include reference #include <cyfxbulklpauto.h> to #include <my_proj.h> Repeat this with my_projdscr.c file.

   

Open the file called .project and replace the project description name from USBBulkLoopAuto to my_proj.  Also search and replace BulkLoopAuto with my_proj.

   

Open the .cproject file and using search and replace, replace BulkLoopAuto with my_proj

Open Eclipse and import this project as described in the FX3 Programming manual. Once imported you can then edit the source code and add files to suit your requirements.

   

Hope this helps.

   

Sodafarl
 

0 Likes
Anonymous
Not applicable

Thanks, It is working now!

0 Likes