cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

What is the maximum achievable throughput of the GPIF bus if all 4 DMA threads are utilized in MULTI + AUTO mode?

0 Likes
4 Replies
Anonymous
Not applicable

Hi,

   

If the USB side application is fast enough then the maximum speed that you can achieve using GPIF II is close to 400MBps.

   

Regards,

   

sai krishna.

0 Likes
Anonymous
Not applicable

 What host controller was used when achieving the 400MB/s?

0 Likes
Anonymous
Not applicable

Hi,

   

I don't think we have done any measurements with the configuration that you are looking for.

   

But as you know the GPIF II interface can run at 100MHz, with 32-bit data bus (400MBps).

   

The practical max speed that we have seen from GPIF to USB side is 357MBps. refer to following application note:

   

http://www.cypress.com/?rID=51581

   

 

   

Win7 64-bit PC with an Intel Z77 Express Chipset is used to take these measurements.

   

Regards,

   

sai kirshna.

0 Likes
Anonymous
Not applicable

Please refer to the following application note to find out the host controller that gave maximum performance:

   

AN86947 - Optimizing USB 3.0 Throughput with EZ-USB® FX3™

   

 

   

Thanks,

   

Sai Krishna.

0 Likes