cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

QsLi_3517121
New Contributor

Hi,

Which API should I call?

Please give an example.

thank you!

0 Likes
1 Solution
alamandaa_16
Moderator
Moderator

Hi,

If any of the CTL[12:0] lines are used for GPIF interface they should not be configured as GPIOs. Similarly if some lines of CTL[12:0] are not used for GPIF they can be overridden to be GPIOs using the CyU3PDeviceGpioOverride call.

Regards,

Anil Srinivas.

View solution in original post

0 Likes
3 Replies
VlKh_2251656
Contributor II

I think, not possible...

May be two pin?

0 Likes
VlKh_2251656
Contributor II

But I could be wrong ...

0 Likes
alamandaa_16
Moderator
Moderator

Hi,

If any of the CTL[12:0] lines are used for GPIF interface they should not be configured as GPIOs. Similarly if some lines of CTL[12:0] are not used for GPIF they can be overridden to be GPIOs using the CyU3PDeviceGpioOverride call.

Regards,

Anil Srinivas.

View solution in original post

0 Likes