cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

How ez-usb-fx2lp automatically loads c2 load eeprom boot(24LC128-16KB-2 bytes address)?

which eeprom will select if i connect two eeprom with same size to fx2lp on I2C bus?

0 Likes
1 Solution
ManaskantD_51
Employee

The EEPROM selection is based on its Slave address. Both the EEPROMs should not have the same I2C slave address. Please refer to the FX2LP Technical Reference Manual or the datasheet to determine the correct slave address to boot from I2C EEPROM.

View solution in original post

1 Reply
ManaskantD_51
Employee

The EEPROM selection is based on its Slave address. Both the EEPROMs should not have the same I2C slave address. Please refer to the FX2LP Technical Reference Manual or the datasheet to determine the correct slave address to boot from I2C EEPROM.

View solution in original post