cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

I already have an existing installation (which i want to keep), therefore i think i cannot install eclipse package offered for FX3.

   

Can someone tell me which additional plug-ins / tools i need for building firmware files in eclipse?

   

What i found so far:

   

- genmakebuilder

   

- ScannerConfigBuilder

   

But where do i get them?

   

The second problem: How to compile a firmware file in eclipse? I often have seen a note that this is described

   

in chapter 11 or so, but where do i find this chapter 11?

   

What i have done so far: File->Import, General->Existing Projects into workspace->Next and select path of .project as root directory. Then Project->BuildProject. But nothing happens...Are my steps correct?

   

Where do i configure the path of the ARM compiler? Or must it be at a fixed location?

0 Likes
2 Replies
RoKl_290166
New Contributor II

Hi,

   

check the FX3 programmers Manual, chapter 12. There is a description about the developement Tools and it's usage.

   

 

   

Regards!

0 Likes
Anonymous
Not applicable

Many thanks for the name of the document. Now i have found the correct chapter, which is indeed very detailed.

   

BTW: Needed Eclipse-Plug-In can be downloaded from

   

http://gnuarmeclipse.sourceforge.net/updates

0 Likes