cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

Now I've used SPI interface to connect a Flash memory which stores the code, can I use this interface to communicate with other chips like FPGA?

   

Thank you!

0 Likes
2 Replies
HeLi_263931
Honored Contributor II

Sure. SPI is a bus system. Just connect MOSI, MISO and SCLK to your second chip and use a separate CS signal for it. But check before whether the SPI clock speed can be handled by both, and that the SPI mode (and all other settings) are the same.

0 Likes
Anonymous
Not applicable

Thanks for your answer:)

0 Likes