Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

Hello, 

   

I have 2 question about developing printer application with FX3

   

 

   

1. Does FX3 support multiple class driver ?  such as description below

   

Using 2 interface descriptor which is Printer class and vendor class, and each interface could transfer Bulk IN, Bulk OUT. 

   

 

   

2. Could you share me any FX3's example driver for printer? 

   

Thank you in advancce.

   

Regards.

0 Likes
1 Reply
Anonymous
Not applicable

Yes, FX3 can have two separate interfaces.

   

We do not have any example for interfacing a printer with FX3.

0 Likes