Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

    I create a fpga design to write data to fx3 based on AN65974 (Slave fifo).

   

    IN my Firmware, I use the function as follows- CyU3PGpifSocketConfigure(0, CY_FX_PRODUCER_PPORT_SOCKET, 6, CyFalse, 1);meawhile flagA have been configured as DMA_ready , flagB be configured as DMA_watermark.

   

    I am able to transfer for a very short amount of time before Flag B remains Low = Buffer Full. oscilloscope both flags go low when the buffer is full but only flag A goes back up to show that the buffer is Not Full. Why does the signal not go back up?

   

    I also used this implementation- CyU3PGpifSocketConfigure(0, CY_FX_PRODUCER_PPORT_SOCKET, 0, CyFalse, 0);When changing the watermark value from 6 to 0 I had no issues and flag B matched up with flag A .

   

Thanks!

0 Likes
1 Reply
Anonymous
Not applicable

We have the same problem. Seems to us that there needs to be transfers one last time even when flag B is low - only then it will return to high. Indicates that this interface only works by workarounds.

0 Likes