cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

 Hello everybody

   

 

   

I am using my fx3 dev kit. Everytime i turn on my computer i need to manually update the driver and Sign in a system file with Driver Signature Enforcement Ovberride. After that i need to reboot my pc. I am really frustrated with this issue. Some times i need to do this a couple of times before i can start working (i get code 10 or code 52 error).

   

 

   

Does any one have a more premanent solution to this issue. 

   

 

   

Thank you in advance

0 Likes
2 Replies
Anonymous
Not applicable

The latest FX3 driver for the DVK is signed so there is no need to do such things. The signed driver is part of the Super Speed USB Suite. If you change anything on the inf file, the signature is broken, of course. But for the DVK and the firmware examples it works very well.

0 Likes
Anonymous
Not applicable

 Where can i download the new driver

0 Likes