cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

AN61345 app note is for interfacing fpga to fx2lp...

if i interface image sensor to fx2lp...what modification i need to do??

or any other app note cypress provide for interfacing image sensor to fx2lp through gpif??

if any...let me know

thank you

0 Likes
1 Solution
ManaskantD_51
Employee

Slave FIFO cannot be used to interface image sensor. The image sensor uses different type of control signals as compared to SlaveFIFO.

View solution in original post

13 Replies
ManaskantD_51
Employee

Slave FIFO cannot be used to interface image sensor. The image sensor uses different type of control signals as compared to SlaveFIFO.

View solution in original post

Anonymous
Not applicable

Any other reference to interface image sensor to fx2lp?

let me know?

0 Likes
ManaskantD_51
Employee

UVC class application is not feasible with FX2LP if the UVC headers are to be added inside FX2LP as the core frequency is only 48 MHz. You will get at max around 2-3 frames per second using UVC class.

Anonymous
Not applicable

my sensor is contineously streaming,i dont need i2c interface also and i

dont need uvc headers also

what can i do now?

0 Likes
ManaskantD_51
Employee

Then you can design the state machine that accepts the image sensor data based on FV and LV and send it to USB.

Anonymous
Not applicable

Then you can design the state machine that accepts the image sensor data

based on FV and LV and send it to USB

-->OK

If i create own stae machine and gpif interface for image sensor...i will

get .c file

can i use this .c file in slavefifo firmware?by doing required

modification??

if its not possible...which firware should i use??

0 Likes
Anonymous
Not applicable

mddd

Then you can design the state machine that accepts the image sensor data

based on FV and LV and send it to USB

-->OK

If i create own stae machine and gpif interface for image sensor...i will

get .c file

can i use this .c file in slavefifo firmware?by doing required

modification??

if its not possible...which firware should i use??

any answers?

0 Likes