CX3 OV5640 RefClock 27 MHz 5M(2592*1944)

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
weli_4835011
Level 1
Level 1
First like given

Hello!

We using cx3 and ov5460 develop a UVC device,and refclk source is 27 MHZ.We want to use it in 2592*1944,3fps (usb 2.0), We don't know how to config the mipi parameters.we need help,thanks.

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.

Hello,

Please find the attached CX3 MIPI receiver settings. Please note that the settings populated under the "CX3 MIPI Interface Configuration" section of the tool can be tuned as per the user's requirements (provided that the values are in min/max range)

You can refer to this KBA Steps to Setup up MIPI CSI Camera Solution with CX3 – KBA225748  to generate the firmware using the tool.

The total bandwidth that can be practically supported by USB 2.0 (high speed/full speed) ~ 25 - 30 MBps

So 2592*1944*1*3 =  30 MBps

Please let me know if any queries on this.

Regards,

Rashi

Regards,
Rashi

View solution in original post

5 Replies
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted

Hello,

Please let me know the following details of the CSI MIPI Transmitter (sensor) so that we could help you with the CX3 MIPI Reciever Configuration settings

CSI Clock (MHz):

Data Lane:

THS - Zero:

THS - Prepare

Frame rate: 3

H Active: 2592

HBlanking:

V active: 1944

V Blanking:

Data Format:

Regards,

Rashi

Regards,
Rashi

thanks !

0 Likes

CSI Clock (MHz): 315 MHZ

Data Lane: 2 Lanes

THS - Zero: 90

THS - Prepare: 70

Frame rate: 3

H Active: 2592

HBlanking: 50

V active: 1944

V Blanking: 5

Data Format: YUY2

0 Likes
lock attach
Attachments are accessible only for community members.

Hello,

Please find the attached CX3 MIPI receiver settings. Please note that the settings populated under the "CX3 MIPI Interface Configuration" section of the tool can be tuned as per the user's requirements (provided that the values are in min/max range)

You can refer to this KBA Steps to Setup up MIPI CSI Camera Solution with CX3 – KBA225748  to generate the firmware using the tool.

The total bandwidth that can be practically supported by USB 2.0 (high speed/full speed) ~ 25 - 30 MBps

So 2592*1944*1*3 =  30 MBps

Please let me know if any queries on this.

Regards,

Rashi

Regards,
Rashi

thank you,it workes

0 Likes