cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Anonymous
Not applicable

the cyfx3s_msc firmware on a SFXS board supports cards of 512MB, 1GB, 2GB, 32GB in size; but doesn't support 4GB or 16GB.

Why ? I also have found no answer in the firmware itself. Any clue ?

0 Likes
3 Replies
alamandaa_16
Moderator
Moderator

Hello,

There is no restrictions on 4GB and 16 GB SD cards.

Please let me know, which SD card is used?

Regards,

Anil Srinivas.

0 Likes
Anonymous
Not applicable

Hi:

I did try SD cards of different vendors, i.e., Transcend, of 4-8-16GB. The cards work as expected when plugged

in another card reader. When I use the cyfx3s_msc firmware (on ztex 2.14 board) for these cards I get:

dmesg:

[  +0.001253] usb-storage 1-1:1.0: USB Mass Storage device detected

[  +0.000184] scsi host119: usb-storage 1-1:1.0

[  +1.002568] scsi 119:0:0:0: Direct-Access     Cypress  FX3S MSC DEMO    0001 PQ: 0 ANSI: 6

[  +0.000823] sd 119:0:0:0: Attached scsi generic sg1 type 0

[  +0.008292] sd 119:0:0:0: [sdb] Attached SCSI removable disk

  lsscsi -s:

[119:0:0:0] disk Cypress FX3S MSC DEMO 0001 /dev/sdb -

As you can see the messages don't contain the size of the cards. On MS Windows

the behaviour is the same. Please notice that cards of smaller or bigger size (the same vendors)

work just fine with this board/firmware.

Best regards,

Ivan

0 Likes
alamandaa_16
Moderator
Moderator

Hi Ivan,

Hope your query has been resolved.

FX3S supports cards of 512MB, 1GB, 2GB, 4GB, 8GB, 16 GB and 32GB.

Regards,

Anil Srinivas.

0 Likes