problem in getting FX2 to work in COM PORT.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello Everyone,

I want to communicate with FPGA through FX2 USB using COM PORT. You can see my code( Virtual.c) down here, COM PORTis getting connected but data is not getting transfer.

This is the link of my firmware. i just changed code in "Virtual.c" file.   http://www.cypress.com/documentation/application-notes/an58764-implementing-virtual-com-port-using-f...

Can anyone guide me throgh this?

------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

#pragma NOIV               // Do not generate interrupt vectors

//-----------------------------------------------------------------------------

//   File:      bulkloop.c

//   Contents:   Hooks required to implement USB peripheral function.

//

//   Copyright (c) 2000 Cypress Semiconductor All rights reserved

//-----------------------------------------------------------------------------

#include "fx2.h"

#include "fx2regs.h"

#include "fx2sdly.h" // SYNCDELAY macro

extern BOOL   GotSUD;         // Received setup data flag

extern BOOL   Sleep;

extern BOOL   Rwuen;

extern BOOL   Selfpwr;

xdata volatile unsigned char D3ON         _at_ 0x9800;

xdata volatile unsigned char D3OFF        _at_ 0x9000;

static int x;

unsigned char duk;

static int bcl,i;

xdata volatile unsigned char D5ON         _at_ 0xB800;

xdata volatile unsigned char D5OFF        _at_ 0xB000;

unsigned char dum;

static int z;

extern BYTE xdata LineCode[7] ;

BYTE   Configuration;      // Current configuration

BYTE   AlternateSetting;   // Alternate settings

void display_product(void);

void TD_Poll(void);

//-----------------------------------------------------------------------------

// Task Dispatcher hooks

//   The following hooks are called by the task dispatcher.

//-----------------------------------------------------------------------------

BOOL DR_SetConfiguration();

 

   BYTE TxByte0,RxByte0;

   BYTE TxByte1,RxByte1;

void transmit(void)// Sends data to SBUF0

{

if (!(EP1OUTCS & 0x02))

{

if(i<bcl)

{

   

SBUF0=EP1OUTBUF;

i++;

dum=D5ON;

  z^=1;

  if (z)

  {dum=D5OFF;}

}

else

{

EP1OUTBC = 0x04;// Arms EP1 endpoint

}

}

}

void  Serial0Init () // serial UART 0 with Timer 2 in mode 1 or high speed baud rate generator

{

      

        SCON0  = 0x5A;     // Set Serial Mode = 1, Recieve enable bit = 1

T2CON  = 0x34;     // Int1 is detected on falling edge, Enable Timer0, Set Timer overflow Flag

if ((LineCode[0] == 0x60) && (LineCode[1] == 0x09 ))   // 2400

{

    RCAP2H = 0xFD;       //  Set TH2 value for timer2

RCAP2L = 0x90;  // baud rate is set to 2400 baud

}

   else if ((LineCode[0] == 0xC0) && (LineCode[1] == 0x12 ))   // 4800

{

    RCAP2H = 0xFE;       //  Set TH2 value for timer2

RCAP2L = 0xC8;  // baud rate is set to 4800 baud

}

else if ((LineCode[0] == 0x80) && (LineCode[1] == 0x25 ))   // 9600

{

    RCAP2H = 0xFF;       //  Set TH2 value for timer2

RCAP2L = 0x64;  // baud rate is set to 9600 baud

}

else if ((LineCode[0] == 0x00) && (LineCode[1] == 0x4B ))   // 19200

{

    RCAP2H = 0xFF;       //  Set TH2 value for timer2

RCAP2L = 0xB2;  // baud rate is set to 19200 baud

}

else if ((LineCode[0] == 0x80) && (LineCode[1] == 0x70 ))   // 28800

{

    RCAP2H = 0xFF;       //  Set TH2 value for timer2

RCAP2L = 0xCC;  // baud rate is set to 28800 baud

}

else if ((LineCode[0] == 0x00) && (LineCode[1] == 0x96 ))   // 38400

{

    RCAP2H = 0xFF;       //  Set TH2 value for timer2

RCAP2L = 0xD9;  // baud rate is set to 38400 baud

}

else if ((LineCode[0] == 0x00) && (LineCode[1] == 0xE1 ))   // 57600

{

    RCAP2H = 0xFF;       //  Set TH2 value for timer2

RCAP2L = 0xE6;  // baud rate is set to 57600 baud

}

        else //if ((LineCode[0] == 0x21) && (LineCode[1] == 0x20 ))   // 115200 (LineCode[0] == 0x00) && (LineCode[1] == 0xC2 ))

{

   RCAP2L = 0xF3;

           RCAP2H = 0xFF;

}

TH2    = RCAP2H; //  Upper 8 bit of 16 bit counter to FF

TL2    = RCAP2L; //  value of the lower 8 bits of timer set to baud rate

     

}

void TD_Init(void)             // Called once at startup

{

 

 

// set the CPU clock to 48MHz

     CPUCS = 0x12; //((CPUCS & ~bmCLKSPD) | bmCLKSPD1) ;

   // set the slave FIFO interface to 48MHz

     IFCONFIG |= 0xCB;

     SYNCDELAY;

   //  REVCTL = 0x00;

   //  SYNCDELAY;

     PINFLAGSAB = 0xE0; // FLAGB - EP6FF

     SYNCDELAY;

     PINFLAGSCD = 0x0B; // FLAGC - EP8EF

     SYNCDELAY;

FIFORESET = 0x80; // activate NAK-ALL to avoid race conditions

SYNCDELAY;       // see TRM section 15.14

    FIFORESET = 0x02;             // reset, FIFO 2

    SYNCDELAY;                    //

    FIFORESET = 0x04;             // reset, FIFO 4

    SYNCDELAY;                    //

    FIFORESET = 0x06;             // reset, FIFO 6

    SYNCDELAY;

FIFORESET = 0x08;             // reset, FIFO 8

SYNCDELAY; //

FIFORESET = 0x00; // deactivate NAK-ALL

SYNCDELAY;

  EP1OUTCFG = 0xA0;    // Configure EP1OUT as BULK EP

SYNCDELAY;

     EP1INCFG = 0xA0;     // Configure EP1IN as BULK IN EP

     SYNCDELAY;                    // see TRM section 15.14

     EP2CFG = 0x02;       // Invalid EP

     SYNCDELAY;                  

     EP4CFG = 0x02;      // Invalid EP

     SYNCDELAY;                  

     EP6CFG = 0xE2;      //

     SYNCDELAY;             

     EP8CFG = 0xA2;      // Configure EP8 as BULK IN EP

     SYNCDELAY;  

     EP8FIFOCFG = 0x00;  // Configure EP8 FIFO in 8-bit Manual Commit mode

     SYNCDELAY;

     EP8FIFOCFG = 0x10;

SYNCDELAY;

     EP6FIFOCFG = 0x08;

SYNCDELAY;

     PORTACFG =  0x40;

     SYNCDELAY;

     T2CON  = 0x34;    

EPIE |= bmBIT3 ;              // Enable EP1 OUT Endpoint interrupts

 

  AUTOPTRSETUP |= 0x01;         // enable dual autopointer feature

  Rwuen = TRUE;                 // Enable remote-wakeup

  EP1OUTBC = 0x04;

ES0 = 1; /* enable serial interrupts */

PS0 = 0; /* set serial interrupts to low priority */

TI = 1; /* clear transmit interrupt */

RI = 0; /* clear receiver interrupt */

EA = 1; /* Enable Interrupts */

     Serial0Init();      // Initialize the Serial Port 0 for the Communication SCO

}

void TD_Poll(void)             // Called repeatedly while the device is idle

{

  // Serial State Notification that has to be sent periodically to the host

  if (!(EP1INCS & 0x02))      // check if EP1IN is available

  {

    EP1INBUF[0] = 0x0A;       // if it is available, then fill the first 10 bytes of the buffer with

EP1INBUF[1] = 0x20;       // appropriate data.

EP1INBUF[2] = 0x00;

EP1INBUF[3] = 0x00;

EP1INBUF[4] = 0x00;

EP1INBUF[5] = 0x00;

EP1INBUF[6] = 0x00;

EP1INBUF[7] = 0x02;

    EP1INBUF[8] = 0x00;

EP1INBUF[9] = 0x00;

  EP1INBC = 10;            // manually commit once the buffer is filled

  }

// recieving the data from the USB Host and send it out through UART

// recieve the data from UART and send it out to the USB Host

}

BOOL TD_Suspend(void)          // Called before the device goes into suspend mode

{

   return(TRUE);

}

BOOL TD_Resume(void)          // Called after the device resumes

{

   return(TRUE);

}

//-----------------------------------------------------------------------------

// Device Request hooks

//   The following hooks are called by the end point 0 device request parser.

//-----------------------------------------------------------------------------

BOOL DR_GetDescriptor(void)

{

   return(TRUE);

}

BOOL DR_SetConfiguration(void)   // Called when a Set Configuration command is received

{

   Configuration = SETUPDAT[2];

   return(TRUE);            // Handled by user code

}

BOOL DR_GetConfiguration(void)   // Called when a Get Configuration command is received

{

   EP0BUF[0] = Configuration;

   EP0BCH = 0;

   EP0BCL = 1;

   return(TRUE);            // Handled by user code

}

BOOL DR_SetInterface(void)       // Called when a Set Interface command is received

{

   AlternateSetting = SETUPDAT[2];

   return(TRUE);            // Handled by user code

}

BOOL DR_GetInterface(void)       // Called when a Set Interface command is received

{

   EP0BUF[0] = AlternateSetting;

   EP0BCH = 0;

   EP0BCL = 1;

   return(TRUE);            // Handled by user code

}

BOOL DR_GetStatus(void)

{

   return(TRUE);

}

BOOL DR_ClearFeature(void)

{

   return(TRUE);

}

BOOL DR_SetFeature(void)

{

   return(TRUE);

}

BOOL DR_VendorCmnd(void)

{

   return(TRUE);

}

//-----------------------------------------------------------------------------

// USB Interrupt Handlers

//   The following functions are called by the USB interrupt jump table.

//-----------------------------------------------------------------------------

// Setup Data Available Interrupt Handler

void ISR_Sudav(void) interrupt 0

{

 

   GotSUD = TRUE;            // Set flag

   EZUSB_IRQ_CLEAR();

   USBIRQ = bmSUDAV;         // Clear SUDAV IRQ

}

// Setup Token Interrupt Handler

void ISR_Sutok(void) interrupt 0

{

   EZUSB_IRQ_CLEAR();

   USBIRQ = bmSUTOK;         // Clear SUTOK IRQ

}

void ISR_Sof(void) interrupt 0

{

   EZUSB_IRQ_CLEAR();

   USBIRQ = bmSOF;            // Clear SOF IRQ

}

void ISR_Ures(void) interrupt 0

{

   if (EZUSB_HIGHSPEED())

   {

      pConfigDscr = pHighSpeedConfigDscr;

      pOtherConfigDscr = pFullSpeedConfigDscr;

   }

   else

   {

      pConfigDscr = pFullSpeedConfigDscr;

      pOtherConfigDscr = pHighSpeedConfigDscr;

   }

 

   EZUSB_IRQ_CLEAR();

   USBIRQ = bmURES;         // Clear URES IRQ

}

void ISR_Susp(void) interrupt 0

{

    Sleep = TRUE;

   EZUSB_IRQ_CLEAR();

   USBIRQ = bmSUSP;

}

void ISR_Highspeed(void) interrupt 0

{

   if (EZUSB_HIGHSPEED())

   {

      pConfigDscr = pHighSpeedConfigDscr;

      pOtherConfigDscr = pFullSpeedConfigDscr;

   }

   else

   {

      pConfigDscr = pFullSpeedConfigDscr;

      pOtherConfigDscr = pHighSpeedConfigDscr;

   }

   EZUSB_IRQ_CLEAR();

   USBIRQ = bmHSGRANT;

}

void ISR_Ep0ack(void) interrupt 0

{

}

void ISR_Stub(void) interrupt 0

{

}

void ISR_Ep0in(void) interrupt 0

{

}

void ISR_Ep0out(void) interrupt 0

{

}

void ISR_Ep1in(void) interrupt 0

{

}

void ISR_Ep1out(void) interrupt 0// Places first byte of EP1 OUT buffer in SBUF0

{

EZUSB_IRQ_CLEAR(); //Clears the USB interrupt

EPIRQ = bmBIT3; //Clears EP1 OUT interrupt request

    while (TI == 1) ;

  i=0;

  bcl=EP1OUTBC;

SBUF0=EP1OUTBUF;

i++;

}

void ISR_Ep2inout(void) interrupt 0

{

}

void ISR_Ep4inout(void) interrupt 0

{

}

void ISR_Ep6inout(void) interrupt 0

{

}

void ISR_Ep8inout(void) interrupt 0

{

}

void ISR_Ibn(void) interrupt 0

{

}

void ISR_Ep0pingnak(void) interrupt 0

{

}

void ISR_Ep1pingnak(void) interrupt 0

{

}

void ISR_Ep2pingnak(void) interrupt 0

{

}

void ISR_Ep4pingnak(void) interrupt 0

{

}

void ISR_Ep6pingnak(void) interrupt 0

{

}

void ISR_Ep8pingnak(void) interrupt 0

{

}

void ISR_Errorlimit(void) interrupt 0

{

}

void ISR_Ep2piderror(void) interrupt 0

{

}

void ISR_Ep4piderror(void) interrupt 0

{

}

void ISR_Ep6piderror(void) interrupt 0

{

}

void ISR_Ep8piderror(void) interrupt 0

{

}

void ISR_Ep2pflag(void) interrupt 0

{

}

void ISR_Ep4pflag(void) interrupt 0

{

}

void ISR_Ep6pflag(void) interrupt 0

{

}

void ISR_Ep8pflag(void) interrupt 0

{

}

void ISR_Ep2eflag(void) interrupt 0

{

}

void ISR_Ep4eflag(void) interrupt 0

{

}

void ISR_Ep6eflag(void) interrupt 0

{

}

void ISR_Ep8eflag(void) interrupt 0

{

}

void ISR_Ep2fflag(void) interrupt 0

{

}

void ISR_Ep4fflag(void) interrupt 0

{

}

void ISR_Ep6fflag(void) interrupt 0

{

}

void ISR_Ep8fflag(void) interrupt 0

{

}

void ISR_GpifComplete(void) interrupt 0

{

}

void ISR_GpifWaveform(void) interrupt 0

{

}

-------------------------------------------------------------------------------------------------------------------------------------------------------------------------

0 Likes
1 Solution
Anonymous
Not applicable

Hello Everyone,

-asserted and deasserted all the signals like in manual( took care of all setup and hold time).

-made PA7 to GND ( as i am working with FLAG B&C only)

-made changes to DSCR.A51, to select proper EP which i am using.

-added Virtual COM PORT descriptor i.e. interface &Header descriptor , ACM,Union &CM Functional descriptor.

- made changes in TD_INIT(), to get it to work according to my selections of all FIFO's and everything.

So everything is working fine.

Thanks for help!

--

Regards,

Avinash

View solution in original post

0 Likes
5 Replies
Anonymous
Not applicable

UPDATE:

FIFO OUT  is happening ( modified DSCR.A51) , I am able to receive data in FPGA.

FIFO IN is  having some problem.

What factors might be reason for problem here?

0 Likes
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello,

Please confirm if my understanding is correct- You are sending out data using a terminal after the FX2LP enumerates as COM port, and then sending the data to the FPGA through the slave FIFO interface and receiving the data in a similar manner. In that case, why are you sending the data over SBUF0? Please check if your endpoints are configured properly in your descriptor file as well.

Best Regards,

Sananya

0 Likes
Anonymous
Not applicable

I dont know how much SBUF0 will create problem, because as TRM section 14.3.4.2 says , we can use it in mode 1 also,right?

0 Likes
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello,

Yes, correct. But as per your firmware, you need to either configure endpoints 6,8 to be of CDC class or commit the data from your EP6 IN endpoint to EP1 IN instead of committing it from SBUF0 so that you can read the data from your FPGA in any terminal emulator.

Best Regards,

Sananya

0 Likes
Anonymous
Not applicable

Hello Everyone,

-asserted and deasserted all the signals like in manual( took care of all setup and hold time).

-made PA7 to GND ( as i am working with FLAG B&C only)

-made changes to DSCR.A51, to select proper EP which i am using.

-added Virtual COM PORT descriptor i.e. interface &Header descriptor , ACM,Union &CM Functional descriptor.

- made changes in TD_INIT(), to get it to work according to my selections of all FIFO's and everything.

So everything is working fine.

Thanks for help!

--

Regards,

Avinash

0 Likes