USB low-full-high speed peripherals Forum Discussions
text.format{('custom.tabs.no.results')}
Dear Sirs and Madams,
Specifically, we are considering a USB connection between the sensor and a personal computer by mounting a USB-UART bridge chip on the sensor side.
If We use an Infineon USB serial device, is it okay to use it as is?
Do we have to get a PID / VID and use that ID?
Also, is it okay to use the Cypress driver as it is, as shown in the KBA91366 below?
KBA91366 URL
Regards,
Show LessHello,
I am using an electroencephalogram (EEG) that uses a CyUSB.sys driver. I am looking to get the incoming EEG data into MATLAB. I have used the code below and am getting this error. I also do not know what to do even if this code worked, how to get data into MATLAB in real-time is even the bigger challenge I am facing.
Error
Message: Arithmetic operation resulted in an overflow.
Source: CyUSB
HelpLink:
Code:
try
CyUSBdll = NET.addAssembly('C:\Cypress\Cypress Suite USB 3.4.7\CyUSB.NET\bin\CyUSB.dll');
catch error
error.message
if(isa(error,'NET.NetException'))
e.ExceptionObject
else
disp('CyUSB.dll already loaded');
return;
end
end
usbDevices = CyUSB.USBDeviceList(CyUSB.CyConst.DEVICES_CYUSB);
PS: I am a psychology student and do know much about drivers and all.
Show LessWhat is the MSL of CY7C68013A-56PVXI? MSL is blank on the website below.
https://www.infineon.com/cms/jp/product/universal-serial-bus-usb-power-delivery-controller/peripheral-controllers/ez-usb-fx2lp/cy7c68013a-56pvxi/
Thanks,
Tetsuo
Hi All !
I am trying to run serial port 1 on my cy7c68013a as this is my hardware requirement and I cannot shift it to serial port 0. I had successfully initialized serial port 0 and am able to use uart at 9600 baud rate.
Can anyone help me in configuring the uart at same baud rate on serial port 1.
For refernece I had attached my code along.
Show LessHi,
I'm using th CYUSBS234 and modifing the examples of the SDK in order to activate and deactivate several GPIOS. I have seen that if the GPIO is configured as Tristate in the Serial Configuration Utility, the api function CySetGpioValue fails.
I haven't seen any function to configurate the GPIO as Drive 0 or Drive 1. So if I want to generate my own production aplication to move those GPIOS , previously I must use the Serial Configuration Utility to configure them as Drive 0/1, isn't it?
Anybody knows if the SDK library allows to configure the GPIOS as Drive0/1 instead of TRISTATE? Because the default configuration of CY7C6511 is Mode 0, with the uart with 6 pins, and all the GPIOS to TRISTATE, or TX/RX LEDs.
By the way, I haven neither seen any function in the sdk to change the uart type to 2 pins, it must be made through the Serial Configuration Utility.
Am I missing something??
Thanks
Show Less
Hello,
I am working with the FX2lp / GPIF and go through the AN57322 (Interfacing SRAM with FX2LP over GPIF)
I wonder about the sequenze "within" a decision point / data action point.
- When will be the databus sampled, either for a read waveform or a write waveform within an IFCLK (rising / falling edge) ?
- When will be the control signals set within an IFCLK ( after/before sampling, rising / falling edge) ?
- When will be the RDY singals be sampled, either asynchrounous (SAS= 0) or synchronous(SAS = 1) within a IFCLK ?
- When will be the logical funtion within a DP finally be executed?
What is the "internal delay" between all the sampling and signal settings?
Getting a better understanding within one IFCLK period, can I assume that IFCLK will be a kind of "trippled" for the sampling, setting CTL signals and following logical functions.
Especially for FIFO waveforms (repeating decision points) this is difficult to understand.
Thanks
Roman
Show LessHello,
I’m Sufiya from Dentals Inc. that is a company making or repairing Dental Sensors. This CY7C68013A-56BAXC is in dental sensor board. Can you provide instructions or and Application Note which details how to program this IC.
Show LessDear Sirs,
Are the ICs CY7C65215 or CY7C65215A qualified AEC Q100 ?
Thank you very much,
Kind regards,
Thierry