USB low-full-high speed peripherals Forum Discussions
Dear cypress experts,
I came a System.OverflowException when build with CyUSB.dll,at win10+x64+VS2012/2013/2015+.net4.0, build as debug+x64
is there a CyUSB.dll for win10+x64+VS2012/2013/VS2015+.net4.0? or could I download the source code of CyUSB.dll and rebuild it?
Thanks for your time。 Looking forward to your response.
By the way, CyUSB.dll in CyUSB Suite 3.4.7 works fine when it's win7+x64+VS2012/2013/2015+.net4.0 or win10+x64+VS2010+.net4.0 or win10+x64+VS2012/2013/2015+.net 3.5. By at win10+x64+VS2012/2013/VS2015+.net4.0, this System.OverflowException will occur.
Show Less
Visual Studio 2015 first doesn't like the project file and requires you to upgrade the project file. Second
when you do get to where you can build it gives 53 errors. I suspect there is some header file missing.
Any ideas ?
Severity Code Description Project File Line Suppression State
Error C2653 'System': is not a class or namespace name Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 3
Error C2871 'Reflection': a namespace with this name does not exist Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 3
Error C2653 'System': is not a class or namespace name Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 4
Error C2871 'CompilerServices': a namespace with this name does not exist Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 4
Error C2337 'AssemblyTitleAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 11
Error C2337 'AssemblyDescriptionAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 12
Error C2337 'AssemblyConfigurationAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 13
Error C2337 'AssemblyCompanyAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 14
Error C2337 'AssemblyProductAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 15
Error C2337 'AssemblyCopyrightAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 16
Error C2337 'AssemblyTrademarkAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 17
Error C2337 'AssemblyCultureAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 18
Error C2337 'AssemblyVersionAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 31
Error C2337 'AssemblyDelaySignAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 55
Error C2337 'AssemblyKeyFileAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 56
Error C2337 'AssemblyKeyNameAttribute': attribute not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\AssemblyInfo.cpp 57
Error C2871 'System': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 8
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 9
Error C2871 'ComponentModel': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 9
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 10
Error C2871 'Collections': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 10
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 11
Error C2871 'Forms': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 11
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 12
Error C2871 'Data': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 12
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 13
Error C2871 'Drawing': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 13
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 14
Error C2871 'Threading': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 14
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 15
Error C2871 'Diagnostics': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 15
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 16
Error C2871 'Reflection': a namespace with this name does not exist Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 16
Error C2059 syntax error: 'public' Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 19
Error C2653 'System': is not a class or namespace name Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 19
Error C2143 syntax error: missing ';' before '{' Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 20
Error C2447 '{': missing function header (old-style formal list?) Streamer c:\cypress\cypress suite usb 3.4.7\cyapi\examples\streamer\Streamer.h 20
Error C2653 'System': is not a class or namespace name Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 14
Error C2871 'Forms': a namespace with this name does not exist Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 14
Error C2653 'System': is not a class or namespace name Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 22
Error C2065 'CurrentThread': undeclared identifier Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 22
Error C2227 left of '->ApartmentState' must point to class/struct/union/generic type Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 22
Error C2065 'STA': undeclared identifier Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 22
Error C2653 'Application': is not a class or namespace name Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 26
Error C2061 syntax error: identifier 'Form1' Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 26
Error C3861 'Run': identifier not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 26
Error C2061 syntax error: identifier 'Exception' Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 28
Error C2310 catch handlers must specify one type Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 28
Error C2653 'MessageBox': is not a class or namespace name Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 30
Error C2065 'e': undeclared identifier Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 30
Error C2227 left of '->StackTrace' must point to class/struct/union/generic type Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 30
Error C2227 left of '->Message' must point to class/struct/union/generic type Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 30
Error C3861 'Show': identifier not found Streamer C:\Cypress\Cypress Suite USB 3.4.7\CyAPI\examples\Streamer\Streamer.cpp 30
Show LessHello,
I need to know if there is a USB cable connected or not. How can i do that. I need this for reading by an FPGA
Thanks for your help
Regards
Franck RAUX
Show LessHello,
I am using CYUSB232 RDK to check the operation of CY7C65213-32LTXI.
After connecting the device to the USB, its TXD line is High.
However, once the port is opened / closed by software (ex. TeraTerm Pro), the TXD line becomes indeterminate(Probably Hi-Z state).
Therefore, incorrect data will be sent to the receiving side.
Is there a way to avoid this situation?
Thanks,
Shimamura
Show LessHello,
I am using CY7C68013A for data transfer between FPGA and PC. I am using internal clock of 48 MHz for Cypress and 100 MHz for FPGA.
So how should i sync. all the signals w.r.t. IFCLK?
Thanks!
--
Regards,
Avinash
Show LessDear Madam/Sir:
After I download FW to Our USB TV dongle, The device manager shows a yellow warning as my attachment. .Can you tell me how to cover this issue?
Thanks
Show Less在新设计的FX 3014单板上增加了调试串口芯片CY7C65215,为什么win7的设备管理器的com口识别出两个串口?并且串口打印不出任何信息。
而官方的SuperSpeed Explorer Kit开发板的CY7C65215的调试口只显示一个串口,打印信息也正常。
我设计的单板原理图和官方的开发板是一样的。请帮忙,多谢。
Show LessHi,
Need a low-power USB, Audio device class 2.0 to I2S bridge,
so looking at FX2LP FX2LP18 to do this in combo with some ARM cortex CPU.
What power consumption should I expect when running say a 44.1/16 bi-directional uac2 stream using hte FX2LP?
Thanks David
Show LessHy
I try to suspend the FX2LP. I set SUSPEND to any value (e.g. 0x10) but it doesn not go to suspend (I check it by TD_Suspend ran or not. or It does not run in that case?)
If a set Sleep = TRUE, TD_Suspend ran and go to sleep. How should I exaclty suspend the FX2LP? An how can I check it?
If FX2LP is suspended, is it enough to send a intterupt/bulk/or any msg from the host to FX2LP to wake up? Because in that case TD_Resume funciton didnot run.
How should I exactly wake up FX2LP?
Thanks,
domi
Show LessDear Madam/Sir:
We use Cypress USBsuite to download iic file to EEPROM(AT24C256),It seems that Only “Universal Serial Bus controller” display with “Cypress EZ-USB FX2LP No EEPROM,” Cypress USBsuite can download iic file , which means 1 EEPROM can only be download once.
How can I download several times to EEPROM?
1、 Device manager里面Universal Serial Bus controller显示Cypress EZ-USB FX2LP No EEPROM(3.4.5000),使用USB Control Center成功download FW(bulkloop.iic)一次
Show Less