cancel
Showing results for 
Search instead for 
Did you mean: 

USB Low-Full-High Speed Peripherals

Anonymous
Not applicable

Is it possible to configure FXLP2 in a way that, once triggered, GPIF continuously flushes endpoint data to external FIFO - that is, without re-arming transaction counter after every 256 cycles (16-bit mode)?

   

In this application there's no in endpoint, so no need for dataflow reversal...

   

- Dejan

0 Likes
1 Reply
Anonymous
Not applicable

dejan,

   

Yes it is possible to continuously transfer the data through gpif interface.You can make your state machine independent of transaction count and instead use flags to make decesions at decesion points in your state machine.If you can elaborate your specific requirements I may be able to help more.

   

-shub

0 Likes