Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

On FX2, with quad buffered EP2 bulk configured as IN

   

The TRM isn't clear if the empty/full signals are conveying state of a single 
512 byte buffer or on all 4 buffers.

   

1) Does the Empty Flag means all 4 buffers are empty? Or just the active buffer?
2) Does the Full Flag mean all 4 buffers are full? Or just the active buffer?

   

The link below suggests the answer is "just the active buffer" for both questions. I just needed to confirm. 

   

http://www.cypress.com/knowledge-base-article/multi-buffering-fx2lp-endpoints

0 Likes
1 Reply
Hemanth
Moderator
Moderator
Moderator
First like given First question asked 750 replies posted

Hi,

The external master typically monitors the ‘empty’ flag (EF) of OUT endpoints and the full (FF) flag of IN endpoints. If the Full Flag is asserted it indicates that no more FIFO buffers are available for the external master to write into. Similarly If the Empty Flag is asserted it indicates that no more FIFO buffers are available for the external master to read from.

Regards,

Hemanth

Hemanth
0 Likes